Other Parts Discussed in Thread: TM4C129ENCPDT, EK-TM4C129EXL, SW-TM4C
Hello,
How can i update firmware in TM4C129ENCPDT MCu through Ethernet??
Is it possible??
Regards
Vidisha
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TM4C129ENCPDT, EK-TM4C129EXL, SW-TM4C
Hello,
How can i update firmware in TM4C129ENCPDT MCu through Ethernet??
Is it possible??
Regards
Vidisha
If you want to use the ROM Bootloader, then first get the IP address that is assigned to the board (this can be figured out by running enet_lwip or similar example first). Next erase the flash of the MCU (you can use "LM Flash Programmer"). Then use "LM Flash Programmer" to program any example from TivaWare (like blinky). Do not use the examples that starts with boot_ (these are for flash based bootloader).
Use the "Help" option of "LM Flash Programmer" for instructions on how to program an application using Ethernet.
If you want to use Flash based bootloader, then the flash based bootloader for EMAC is present in the folder "./examples/boards/dk-tm4c129x/boot_emac_flash". Program this binary using JTAG. Then follow the above steps to program an application using Ethernet. Applications need to be built specifically to work with Flash based bootloader. These application can be found in the folder "./examples/boards/dk-tm4c129x/". Use the examples "boot_demo_emac_flash" and "boot_demo_flash".
Thanks,
Sai
Hi,
Thanks for replying!!!
Do i need to program Boot loader every time ? or will it stay in Flash permanently?
Actually i want a Boot loader which runs upon some mechanism like pressing a "Reset button" then it must allow us to update our application code.
Then follow the above steps to program an application using Ethernet ??
You mean every time i must erase the Flash and program the new application code?
Thanks & Regards
vidisha
The whole purpose of a bootloader is so that it can be programmed once, and then using this bootloader, the application can be updated whenever necessary.
So program the Flash based bootloader once (using JTAG) then using this bootloader, program the application when ever needed.
To program the application (using the bootloader over Ethernet), you will need the IP address of the board. You can get this information by
Hope this time I did a better job at explaining.
Thanks,
Sai
Hello sai,
ok sorry for not being clear..
As said my board is TM4C129EXL which has TM4C129ENCPDT MCU but i couldn't find ethernet bootloader code for this device so,
I got the codes from Git hub for DK-TM4C129X which has TM4C129XNCZAD MCU.
I know there is a difference between Ek-TM4C129EXL & DK-TM4C129X so even i changed the make file to work with my device, but no output.
https://github.com/yuvadm/tiva-c/tree/master/boards/dk-tm4c129x/boot_emac_flash
Then i uploaded boot_emac_flash into my device using LM Flash programmer.
It showed me successfully programmed - 4,440 bytes.
Then i tried to load the example code "boot_demo_emac_flash" which is again for DK-TM4C129X which has LCD screen and my board doesn't hav LCD screen.
so first thing i want to know why only few codes work with ethernet bootloader like boot_demo_emac_flash? why not Blinky?
github.com/.../boot_demo_emac_flash
so i tried with Blinky project as my board doesn't hav LCD screen and after uploading the example code it shows "attempting to connect" for long time which means the code is not correct..
so plz guide me where i am going wrong.
Regards
Vidisha

Hello Vidisha,
I am not sure why you are using the code from the Github. That code is not from TI. It might be a copy of a TivaWare example, that might have been modified.
I would recommend downloading and using TivaWare from www.ti.com/tool/sw-tm4c.
I have programmed the Ethernet bootloader present in the "./examples/boards/dk-tm4c129x/boot_emac_flash" onto a EK-TM4C129EXL board, without any changes, using "LM FLASH Programmer" over the ICDI interface. Then I programmed a binary file using this bootloader through "LM Flash Programmer's" (You will need the MAC address and IP address of the board). Note that this binary won't run, and would generate a fault, because it was not built to run with the Ethernet bootloader but it demonstrates that the Ethernet bootloader for the DK-TM4C129X board (in TivaWare) will work with the EK-TM4C129EXL board without any change.
You will have to modify the examples in the folder "./examples/boards/dk-tm4c129x/boot_demo_flash" and "./examples/boards/dk-tm4c129x/boot_demo_emac_flash" to work with EK-TM4C129EXL.
I would also recommend reading the TivaWare Boot Loader User's Guide before modifying the application code that works with the Flash based bootloader.
Thanks,
Sai
Hi sai,
Can you tell me what modifications are to done to Application code i.e boot_demo_emac_flash inorder to make it work with EK-TM4C129EXL ?
Do you have the modified application code for EK-TM4C129EXL.?
If yes plz send me na meanwhile i'll also try to modify it.
Thanks
vidisha