This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129 Hibernation Module Interrupt every 5 Minutes

Other Parts Discussed in Thread: TM4C129ENCPDT

Hi,

i've got the Hibernate Module running in 24h Mode.

Is there a way to set a Match register that calls in interrupt every 5 Minutes.

Times: 4:00, 4:05, 4:10 and so on..

I can't use a normal Timer for that because i want it syncronized with the Rea Time Clock.

Thank you