Hi all,
I have been comparing the HALCoGen reset code against the RM57L843 documentation and found some discrepancies. I am wondering if you can explain whether these are HALCoGen problems or if I am just not understanding something.
This code was generated by HALCoGen 04.05.02 for the Hercules RM57L843.
Question 1: HL_system.h provides the following enum of reset sources:
typedef enum { POWERON_RESET = 0x8000U, /**< Alias for Power On Reset */ OSC_FAILURE_RESET = 0x4000U, /**< Alias for Osc Failure Reset */ WATCHDOG_RESET = 0x2000U, /**< Alias for Watch Dog Reset */ WATCHDOG2_RESET = 0x1000U, /**< Alias for Watch Dog 2 Reset */ DEBUG_RESET = 0x0800U, /**< Alias for Debug Reset */ INTERCONNECT_RESET = 0x0080U, /**< Alias for Interconnect Reset */ CPU1_RESET = 0x0040U, /**< Alias for CPU 1 Reset */ CPU0_RESET = 0x0020U, /**< Alias for CPU 0 Reset */ SW_RESET = 0x0010U, /**< Alias for Software Reset */ EXT_RESET = 0x0008U, /**< Alias for External Reset */ NO_RESET = 0x0000U /**< Alias for No Reset */ }resetSource_t;
This matches the SYSESR table in spnu562, 2.5.1.46, with one key difference: spnu562 marks bit 6 as "reserved", while HL_system.c marks it as "CPU1_RESET". Which is correct?
Question 2: HL_system.c provides a getResetSource() function, containing a large if-else that looks like it should have cases for each possible resetSource_t. However, it does not - it is missing a handler for INTERCONNECT_RESET. This falls through to the "else" and is treated as NO_RESET. Is this behavior deliberate?
resetSource_t getResetSource(void) { register resetSource_t rst_source; ...
Question 3: HL_sys_startup.c contains a switch statement that branches on getResetSource(). Like HL_system.c, it is missing a case for INTERCONNECT_RESET, but on top of that, it is also missing a case for WATCHDOG2_RESET. (This falls through to the "default", which does nothing). Is this behavior deliberate?
switch(getResetSource()) { case POWERON_RESET: ...
Thanks for any insight,
Peter