Other Parts Discussed in Thread: EK-TM4C1294XL
Hello,
To get straight to the point, I'm using the EK-TM4C1294XL launchpad with the IR LED and receiver from the Boe-Bot kit (Board of Education development board). I seems to have everything working okay, but the only issue I'm having (if it really is an issue) is that when I place my hand in front of the LED as a reflector for the IR to reach the receiver, the receiver is displaying 0's, which means it is indeed detecting something. BUT after about 3 seconds, the 0's turn back to 1's (not detecting) while my hand is still in the way. Also, the sensor only detects when I move my hand up and down. When I move my hand horizontally toward the sensor, it does not detect. Does anyone have an idea on what might be the problem?
Thanks!