Other Parts Discussed in Thread: HALCOGEN
Hi All,
I am satring out with Hercules MCU's and am lost at the moment. please help and advise
I have a TMS570LS4x Launchpad and istalled CCS and Halcogen I managed to generate the files for the HET to Blink the led on NHET8 pin
so I guess the tools are working.
I am very new to Ti Controllers has worked with another vendor on 16bit t mico's however I need some help to understand where to find example
code or a document that explains how to use the functions generated in Halcogen for example the HET in the project 0 generate a constant PWM frequency with a fixed Dutycycle ,I saw that in the genarted file there is a function to set the duty what is not clear is the parameter list for the function as it menstion RAM1 or RAM2
and then the duty cycle in percent and the pwm channle the last two are more or less clear butr ,what RAM shoud I pass
I need examples for the different peripherals the documentation on the weg page AP note just tells how to use Halcogen.
Please how do I start to learn these tools and complex mcu any advise is appreciated
Regards.
Peter