Hi all,
I have a follow-up question about ESM1.90 that I did not ask in my previous thread:
I am still getting ESM 1.90's from time to time. They are not readily reproducible, but I normally get at least a few a day. I have confirmed this behavior on multiple boards, both HDK's and custom PCB's, using RM57's from SIlicon Revisions A and B.
This is indeed a benchtop environment with no (known?) radiation sources nearby to cause legitimate bit flips. Besides, in that case I'd expect occasional bit flips in all the modules, not just SYS.
Is there any additional information available, such as an "error details" register that I can read that would specifically tell me which SYS register(s) flipped bits to trigger the ESM1.90? I understand that in the case of a SRAM, CPU, flash or interconnect fault, I could read the fault address from the EPC, but the EPC's section of spnu562 does not mention any diagnostics of the SYS module.
Basically, I'm looking for ways to confirm that the ESM1.90 indicates a real soft error in the SYS module (not an error in the diagnostics), and then identify any patterns in the fault details that might help me find the root cause.
Any suggestions?
Best,
Peter