This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PWM OUTPUT from 3.3 to 5 V

Hello,

I am having an issue with setting up a port. I am currently trying to use PF1 which relates to PW5 (Gen2) to generate a pulse width signal to send to a motor controller. Now the issue is with the motor controller. It is expecting a 5V PWM signal and the TIVA C processor only is outputting a 3.36V pwm signal. I have read a lot about the ports and it seems 3.36V is the best i will be able to get. So before i have to design something to increase the voltage i just wanted to double check that there is no way to output a 5V pwm signal using the TIVA-C Tm4c micro controller.