This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM48 Micro controller 1 sec delay generation with simple function.

Hi,

I need to generate different delay for my application based on the input from another processor. How to generate a delay of 1, 2 sec etc. What is the relation between clock speed of controller and the delay? I need support. I am using RM48 Microcontroller (I found that clock speed of the microcontroller is 220MHz and the VCLK speed of HET is 110MHZ. How to create a simple delay function? 

Thanks and Regards

K.Manjunathan

PSGIAS