Hello
I am currently using the schematic of the DK mentionned higher for one of our project.
I have a few questions:
1./ PAGE 1, on the extreme left there is a single capacitor alone named C2, is it a decoupling capacitor ? or what is it doing alone here ? where should it be placed on the PCB layout (close to a pîn in particular) ?
2./Still on page 1, I see on the JTAG, the signal EXTDBG it goes to the bus for debugging but I don't see on which pin it is landing on the MCU
3./ On page 2 there is the CAN transceiver, on the schematic it got only one cpaacitor on VCC. however if you look at the datasheet of this component here :
on page 25, you find out a layout that indicate several other capacitor and resistor to add around the component. Can you confirm the schematic of the DK is proper ?
4./ Page 2, on the micro SD card area, there is capacitor C5 which is also isolated from any connection, can you please clarify the use of this capacitor and the position on the layout (is it supposed to be close to VDD ?)
5./ Page 3, two converter 5V to 3V and 3.3V are used , one is U8 and one is U5, they seems to do the sames things, why using two, and not only one ? Can you also confirmed they are used for power the circuit from a 5V usb power port ?
6./On all pages, there are some square pin named H? can you confirm those are test point ?
7../ On page 3, on the right there is U15. I don't understand the use of it., I have read this :
but I don't see why we use this.
8./ PAGE 3, there is a whole line of decoupling capacitor, they have different value. How do we know which capacitor should go on which pin ?
9./ PAGE 3 there is resistor R34 value 0.1, can you confirm the value and unit ?
10./ I have difficulties to understand what is the differences using ICDI vs JTAG. Is it just the fact that we can use USB port to load firmware into the chip that make it different with ICDI ?
Thank you in advance for your answers and clarifications (I know there are a lot of questions :) )