This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129X Dev kit GPIO not responding as expected!

Hi,

I am trying to control 8 or 10 GPIO's from from a web server.

I have started to modify the enet_io example code to hard code some of the available GPIO's on the board ( for example from connector J29 and J30 Pins PN0 , PN1, PN2...etc). Specifically I am modifying the IO.c ,I used the API given in the document to configure the port to GPIO Output (  ROM_GPIOPinTypeGPIOOutput(IO_PORT_BASE_N, IO_PIN_0); )  and ROM_GPIOPinWrite(IO_PORT_BASE_N, IO_PIN_0, 1); )

I was able to see the PN0 high after falshing the code but none of the other GPIO's are high when Api's are called similarly to this.

Any thoughts on what's need to be done to configure the GPIO's available on the board to be able to make it usable for my application.

Any Example code would be much appreciated.

Thanks,

  • Hello Ramana,

    Is it possible to upload your project so that we can have a look at it? This will probably be the quickest way to find an answer to your question.
  • //*****************************************************************************
    //
    // enet_io.c - I/O control via a web server.
    //
    // Copyright (c) 2007-2013 Texas Instruments Incorporated.  All rights reserved.
    // Software License Agreement
    // 
    // Texas Instruments (TI) is supplying this software for use solely and
    // exclusively on TI's microcontroller products. The software is owned by
    // TI and/or its suppliers, and is protected under applicable copyright
    // laws. You may not combine this software with "viral" open-source
    // software in order to form a larger program.
    // 
    // THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
    // NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
    // NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
    // CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
    // DAMAGES, FOR ANY REASON WHATSOEVER.
    // 
    // This is part of revision 2.0.1.11577 of the DK-TM4C129X Firmware Package.
    //
    //*****************************************************************************
    #include <stdbool.h>
    #include <stdint.h>
    #include <string.h>
    #include "inc/hw_ints.h"
    #include "inc/hw_memmap.h"
    #include "inc/hw_nvic.h"
    #include "inc/hw_types.h"
    #include "driverlib/flash.h"
    #include "driverlib/gpio.h"
    #include "driverlib/interrupt.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/systick.h"
    #include "driverlib/timer.h"
    #include "driverlib/rom.h"
    #include "utils/locator.h"
    #include "utils/lwiplib.h"
    #include "utils/uartstdio.h"
    #include "utils/ustdlib.h"
    #include "httpserver_raw/httpd.h"
    #include "grlib/grlib.h"
    #include "drivers/kentec320x240x16_ssd2119.h"
    #include "drivers/pinout.h"
    #include "io.h"
    #include "cgifuncs.h"
    #include "drivers/frame.h"
    
    //*****************************************************************************
    //
    //! \addtogroup example_list
    //! <h1>Ethernet-based I/O Control (enet_io)</h1>
    //!
    //! This example application demonstrates web-based I/O control using the
    //! Tiva Ethernet controller and the lwIP TCP/IP Stack.  DHCP is used to
    //! obtain an Ethernet address.  If DHCP times out without obtaining an
    //! address, a static IP address will be chosen using AutoIP.  The address that
    //! is selected will be shown on the QVGA display allowing you to access the
    //! internal web pages served by the application via your normal web browser.
    //!
    //! Two different methods of controlling board peripherals via web pages are
    //! illustrated via pages labeled ``IO Control Demo 1'' and ``IO Control
    //! Demo 2'' in the navigation menu on the left of the application's home page.
    //! In both cases, the example allows you to toggle the state of the user LED
    //! on the board and set the speed of a graphical animation on the display.
    //!
    //! ``IO Control Demo 1'' uses JavaScript running in the web browser to send
    //! HTTP requests for particular special URLs.  These special URLs are
    //! intercepted in the file system support layer (io_fs.c) and used to
    //! control the LED and animation.  Responses generated by the board are
    //! returned to the browser and inserted into the page HTML dynamically by
    //! more JavaScript code.
    //!
    //! ``IO Control Demo 2'' uses standard HTML forms to pass parameters to CGI
    //! (Common Gateway Interface) handlers running on the board.  These handlers
    //! process the form data and control the animation and LED as requested before
    //! sending a response page (in this case, the original form) back to the
    //! browser.  The application registers the names and handlers for each of its
    //! CGIs with the HTTPD server during initialization and the server calls
    //! these handlers after parsing URL parameters each time one of the CGI URLs
    //! is requested.
    //!
    //! Information on the state of the various controls in the second demo is
    //! inserted into the served HTML using SSI (Server Side Include) tags which
    //! are parsed by the HTTPD server in the application.  As with the CGI
    //! handlers, the application registers its list of SSI tags and a handler
    //! function with the web server during initialization and this handler is
    //! called whenever any registered tag is found in a .shtml, .ssi, .shtm or
    //! .xml file being served to the browser.
    //!
    //! In addition to LED and animation speed control, the second example also
    //! allows a line of text to be sent to the board for display on the LCD
    //! panel.  This is included to illustrate the decoding of HTTP text strings.
    //!
    //! Note that the web server used by this example has been modified from the
    //! example shipped with the basic lwIP package.  Additions include SSI and
    //! CGI support along with the ability to have the server automatically insert
    //! the HTTP headers rather than having these built in to the files in the
    //! file system image.
    //!
    //! Source files for the internal file system image can be found in the ``fs''
    //! directory.  If any of these files are changed, the file system image
    //! (io_fsdata.h) should be rebuilt by running the following command from the
    //! enet_io directory:
    //!
    //! ../../../../tools/bin/makefsfile -i fs -o io_fsdata.h -r -h -q
    //!
    //! For additional details on lwIP, refer to the lwIP web page at:
    //! http://savannah.nongnu.org/projects/lwip/
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // Defines for setting up the system clock.
    //
    //*****************************************************************************
    #define SYSTICKHZ               100
    #define SYSTICKMS               (1000 / SYSTICKHZ)
    
    //*****************************************************************************
    //
    // Interrupt priority definitions.  The top 3 bits of these values are
    // significant with lower values indicating higher priority interrupts.
    //
    //*****************************************************************************
    #define SYSTICK_INT_PRIORITY    0x80
    #define ETHERNET_INT_PRIORITY   0xC0
    
    //*****************************************************************************
    //
    // A set of flags.  The flag bits are defined as follows:
    //
    //     0 -> An indicator that the animation timer interrupt has occurred.
    //
    //*****************************************************************************
    #define FLAG_TICK            0
    static volatile unsigned long g_ulFlags;
    
    //*****************************************************************************
    //
    // The graphics context used by the application.
    //
    //*****************************************************************************
    tContext g_sContext;
    
    //*****************************************************************************
    //
    // The Y extent of the box used to display the text string sent from the
    // remote web browser.
    //
    //*****************************************************************************
    #define TEXT_BOX_TOP        140
    #define TEXT_BOX_BOTTOM     184
    
    //*****************************************************************************
    //
    // The position and size of the box used to display the simple animation.
    //
    //*****************************************************************************
    #define ANIM_TOP            210
    #define ANIM_HEIGHT         20
    #define ANIM_LEFT           40
    #define ANIM_WIDTH          (320 - (2 * ANIM_LEFT))
    
    //*****************************************************************************
    //
    // The RGB value we use to change the color each time the animated bar cycles
    // back to the start.
    //
    //*****************************************************************************
    #define COLOR_INCREMENT     0x00306040
    
    //*****************************************************************************
    //
    // Position and movement granularity for the status indicator shown while
    // the IP address is being determined.
    //
    //*****************************************************************************
    #define STATUS_X     40
    #define STATUS_Y     50
    #define MAX_STATUS_X (320 - (2 * STATUS_X))
    #define ANIM_STEP_SIZE   8
    
    //*****************************************************************************
    //
    // External Application references.
    //
    //*****************************************************************************
    extern void httpd_init(void);
    
    //*****************************************************************************
    //
    // SSI tag indices for each entry in the g_pcSSITags array.
    //
    //*****************************************************************************
    #define SSI_INDEX_LEDSTATE  0
    #define SSI_INDEX_FORMVARS  1
    #define SSI_INDEX_SPEED     2
    
    //*****************************************************************************
    //
    // This array holds all the strings that are to be recognized as SSI tag
    // names by the HTTPD server.  The server will call SSIHandler to request a
    // replacement string whenever the pattern <!--#tagname--> (where tagname
    // appears in the following array) is found in ".ssi", ".shtml" or ".shtm"
    // files that it serves.
    //
    //*****************************************************************************
    static const char *g_pcConfigSSITags[] =
    {
        "LEDtxt",        // SSI_INDEX_LEDSTATE
        "FormVars",      // SSI_INDEX_FORMVARS
        "speed"          // SSI_INDEX_SPEED
    };
    
    //*****************************************************************************
    //
    // The number of individual SSI tags that the HTTPD server can expect to
    // find in our configuration pages.
    //
    //*****************************************************************************
    #define NUM_CONFIG_SSI_TAGS     (sizeof(g_pcConfigSSITags) / sizeof (char *))
    
    //*****************************************************************************
    //
    // Prototypes for the various CGI handler functions.
    //
    //*****************************************************************************
    static char *ControlCGIHandler(int32_t iIndex, int32_t i32NumParams, char *pcParam[],
                                  char *pcValue[]);
    static char *SetTextCGIHandler(int32_t iIndex, int32_t i32NumParams, char *pcParam[],
                                  char *pcValue[]);
    
    //*****************************************************************************
    //
    // Prototype for the main handler used to process server-side-includes for the
    // application's web-based configuration screens.
    //
    //*****************************************************************************
    static int32_t SSIHandler(int32_t iIndex, char *pcInsert, int32_t iInsertLen);
    
    //*****************************************************************************
    //
    // CGI URI indices for each entry in the g_psConfigCGIURIs array.
    //
    //*****************************************************************************
    #define CGI_INDEX_CONTROL       0
    #define CGI_INDEX_TEXT          1
    
    //*****************************************************************************
    //
    // This array is passed to the HTTPD server to inform it of special URIs
    // that are treated as common gateway interface (CGI) scripts.  Each URI name
    // is defined along with a pointer to the function which is to be called to
    // process it.
    //
    //*****************************************************************************
    static const tCGI g_psConfigCGIURIs[] =
    {
        { "/iocontrol.cgi", (tCGIHandler)ControlCGIHandler }, // CGI_INDEX_CONTROL
        { "/settxt.cgi", (tCGIHandler)SetTextCGIHandler }     // CGI_INDEX_TEXT
    };
    
    //*****************************************************************************
    //
    // The number of individual CGI URIs that are configured for this system.
    //
    //*****************************************************************************
    #define NUM_CONFIG_CGI_URIS     (sizeof(g_psConfigCGIURIs) / sizeof(tCGI))
    
    //*****************************************************************************
    //
    // The file sent back to the browser by default following completion of any
    // of our CGI handlers.  Each individual handler returns the URI of the page
    // to load in response to it being called.
    //
    //*****************************************************************************
    #define DEFAULT_CGI_RESPONSE    "/io_cgi.ssi"
    
    //*****************************************************************************
    //
    // The file sent back to the browser in cases where a parameter error is
    // detected by one of the CGI handlers.  This should only happen if someone
    // tries to access the CGI directly via the broswer command line and doesn't
    // enter all the required parameters alongside the URI.
    //
    //*****************************************************************************
    #define PARAM_ERROR_RESPONSE    "/perror.htm"
    
    #define JAVASCRIPT_HEADER                                                     \
        "<script type='text/javascript' language='JavaScript'><!--\n"
    #define JAVASCRIPT_FOOTER                                                     \
        "//--></script>\n"
    
    //*****************************************************************************
    //
    // Timeout for DHCP address request (in seconds).
    //
    //*****************************************************************************
    #ifndef DHCP_EXPIRE_TIMER_SECS
    #define DHCP_EXPIRE_TIMER_SECS  45
    #endif
    
    //*****************************************************************************
    //
    // The positions of the circles in the animation used while waiting for an IP
    // address.
    //
    //*****************************************************************************
    const int32_t g_ppi32CirclePos[][2] =
    {
        {
            12, 0
        },
        {
            8, -9
        },
        {
            0, -12
        },
        {
            -8, -9
        },
        {
            -12, 0
        },
        {
            -8, 9
        },
        {
            0, 12
        },
        {
            8, 9
        }
    };
    
    //*****************************************************************************
    //
    // The colors of the circles in the animation used while waiting for an IP
    // address.
    //
    //*****************************************************************************
    const uint32_t g_pui32CircleColor[] =
    {
        0x111111,
        0x333333,
        0x555555,
        0x777777,
        0x999999,
        0xbbbbbb,
        0xdddddd,
        0xffffff,
    };
    
    //*****************************************************************************
    //
    // The current color index for the animation used while waiting for an IP
    // address.
    //
    //*****************************************************************************
    uint32_t g_ui32ColorIdx;
    
    //*****************************************************************************
    //
    // The current IP address.
    //
    //*****************************************************************************
    uint32_t g_ui32IPAddress;
    
    //*****************************************************************************
    //
    // The application's graphics context.
    //
    //*****************************************************************************
    tContext g_sContext;
    
    //*****************************************************************************
    //
    // The system clock frequency.  Used by the SD card driver.
    //
    //*****************************************************************************
    uint32_t g_ui32SysClock;
    
    
    //*****************************************************************************
    //
    // The error routine that is called if the driver library encounters an error.
    //
    //*****************************************************************************
    #ifdef DEBUG
    void
    __error__(char *pcFilename, uint32_t ui32Line)
    {
    }
    #endif
    
    //*****************************************************************************
    //
    // This CGI handler is called whenever the web browser requests iocontrol.cgi.
    //
    //*****************************************************************************
    static char *
    ControlCGIHandler(int32_t iIndex, int32_t i32NumParams, char *pcParam[], char *pcValue[])
    {
        int32_t i32LEDState, i32Speed;
        bool bParamError;
    
        //
        // We have not encountered any parameter errors yet.
        //
        bParamError = false;
    
        //
        // Get each of the expected parameters.
        //
        i32LEDState = FindCGIParameter("LEDOn", pcParam, i32NumParams);
        i32Speed = GetCGIParam("speed_percent", pcParam, pcValue, i32NumParams,
                             &bParamError);
    
        //
        // Was there any error reported by the parameter parser?
        //
        if(bParamError || (i32Speed < 0) || (i32Speed > 100))
        {
            return(PARAM_ERROR_RESPONSE);
        }
    
        //
        // We got all the parameters and the values were within the expected ranges
        // so go ahead and make the changes.
        //
        io_set_led((i32LEDState == -1) ? false : true);
        io_set_animation_speed(i32Speed);
    
        //
        // Send back the default response page.
        //
        return(DEFAULT_CGI_RESPONSE);
    }
    
    //*****************************************************************************
    //
    // This CGI handler is called whenever the web browser requests settxt.cgi.
    //
    //*****************************************************************************
    static char *
    SetTextCGIHandler(int32_t i32Index, int32_t i32NumParams, char *pcParam[], char *pcValue[])
    {
        long lStringParam;
        char pcDecodedString[48];
        tRectangle sRect;
    
        //
        // Find the parameter that has the string we need to display.
        //
        lStringParam = FindCGIParameter("DispText", pcParam, i32NumParams);
    
        //
        // If the parameter was not found, show the error page.
        //
        if(lStringParam == -1)
        {
            return(PARAM_ERROR_RESPONSE);
        }
    
        //
        // The parameter is present. We need to decode the text for display.
        //
        DecodeFormString(pcValue[lStringParam], pcDecodedString, 48);
    
        //
        // Erase the previous string and overwrite it with the new one.
        //
        sRect.i16XMin = 15;
        sRect.i16XMax = GrContextDpyWidthGet(&g_sContext) - 15 -1 ;
        sRect.i16YMin = TEXT_BOX_TOP + 6;
        sRect.i16YMax = TEXT_BOX_BOTTOM - 2;
        GrContextForegroundSet(&g_sContext, ClrBlack);
        GrRectFill(&g_sContext, &sRect);
    
        //
        // Now draw the new string after setting the clipping rectangle.
        //
        GrContextClipRegionSet(&g_sContext, &sRect);
        GrContextForegroundSet(&g_sContext, ClrYellow);
        GrStringDrawCentered(&g_sContext, pcDecodedString, -1,
                             (sRect.i16XMin + sRect.i16XMax) / 2,
                             (sRect.i16YMin + sRect.i16YMax) / 2, 0);
    
        //
        // Reset the clipping rectangle to the full screen.
        //
        sRect.i16XMin = 0;
        sRect.i16XMax = GrContextDpyWidthGet(&g_sContext) - 1;
        sRect.i16YMin = 0;
        sRect.i16YMax = GrContextDpyHeightGet(&g_sContext) - 1;
        GrContextClipRegionSet(&g_sContext, &sRect);
    
        //
        // Tell the HTTPD server which file to send back to the client.
        //
        return(DEFAULT_CGI_RESPONSE);
    }
    
    //*****************************************************************************
    //
    // This function is called by the HTTP server whenever it encounters an SSI
    // tag in a web page.  The iIndex parameter provides the index of the tag in
    // the g_pcConfigSSITags array. This function writes the substitution text
    // into the pcInsert array, writing no more than iInsertLen characters.
    //
    //*****************************************************************************
    static int32_t
    SSIHandler(int32_t iIndex, char *pcInsert, int32_t iInsertLen)
    {
        //
        // Which SSI tag have we been passed?
        //
        switch(iIndex)
        {
            case SSI_INDEX_LEDSTATE:
                io_get_ledstate(pcInsert, iInsertLen);
                break;
    
            case SSI_INDEX_FORMVARS:
                usnprintf(pcInsert, iInsertLen,
                          "%sls=%d;\nsp=%d;\n%s",
                          JAVASCRIPT_HEADER,
                          io_is_led_on(),
                          io_get_animation_speed(),
                          JAVASCRIPT_FOOTER);
                break;
    
            case SSI_INDEX_SPEED:
                io_get_animation_speed_string(pcInsert, iInsertLen);
                break;
    
            default:
                usnprintf(pcInsert, iInsertLen, "??");
                break;
        }
    
        //
        // Tell the server how many characters our insert string contains.
        //
        return(strlen(pcInsert));
    }
    
    //*****************************************************************************
    //
    // The interrupt handler for the SysTick interrupt.
    //
    //*****************************************************************************
    void
    SysTickIntHandler(void)
    {
        //
        // Call the lwIP timer handler.
        //
        lwIPTimer(SYSTICKMS);
    }
    
    //*****************************************************************************
    //
    // The interrupt handler for the timer used to pace the animation.
    //
    //*****************************************************************************
    void
    AnimTimerIntHandler(void)
    {
        //
        // Clear the timer interrupt.
        //
        ROM_TimerIntClear(TIMER2_BASE, TIMER_TIMA_TIMEOUT);
    
        //
        // Indicate that a timer interrupt has occurred.
        //
        HWREGBITW(&g_ulFlags, FLAG_TICK) = 1;
    }
    
    //*****************************************************************************
    //
    // Display an lwIP type IP Address.
    //
    //*****************************************************************************
    void
    DisplayIPAddress(uint32_t ui32Addr, uint32_t ui32Col, uint32_t ui32Row)
    {
        char pcBuf[16];
    
        //
        // Convert the IP Address into a string.
        //
        usprintf(pcBuf, "%d.%d.%d.%d", ui32Addr & 0xff, (ui32Addr >> 8) & 0xff,
                 (ui32Addr >> 16) & 0xff, (ui32Addr >> 24) & 0xff);
    
        //
        // Display the string.
        //
        GrStringDraw(&g_sContext, pcBuf, -1, ui32Col, ui32Row, false);
    }
    
    //*****************************************************************************
    //
    // Required by lwIP library to support any host-related timer functions.
    //
    //*****************************************************************************
    void
    lwIPHostTimerHandler(void)
    {
        uint32_t ui32Idx, ui32NewIPAddress, ui32Width;
        tRectangle sRect;
    
        //
        // Get the width and height of the display.
        //
        ui32Width = GrContextDpyWidthGet(&g_sContext);
    
        //
        // Get the current IP address.
        //
        ui32NewIPAddress = lwIPLocalIPAddrGet();
    
        //
        // See if the IP address has changed.
        //
        if(ui32NewIPAddress != g_ui32IPAddress)
        {
            //
            // Clear the display.
            //
            sRect.i16XMin = STATUS_X;
            sRect.i16YMin = STATUS_Y - 22;
            sRect.i16XMax = MAX_STATUS_X;
            sRect.i16YMax = TEXT_BOX_TOP - 10;
            GrContextForegroundSet(&g_sContext, ClrBlack);
            GrRectFill(&g_sContext, &sRect);
            GrContextForegroundSet(&g_sContext, ClrWhite);
    
            //
            // See if there is an IP address assigned.
            //
            if(ui32NewIPAddress == 0xffffffff)
            {
                //
                // Indicate that there is no link.
                //
                GrStringDrawCentered(&g_sContext, "Waiting for link", -1,
                                     ui32Width / 2, STATUS_Y, false);
            }
            else if(ui32NewIPAddress == 0)
            {
                //
                // There is no IP address, so indicate that the DHCP process is
                // running.
                //
                GrStringDrawCentered(&g_sContext, "Waiting for IP address", -1,
                                     ui32Width / 2, STATUS_Y, false);
            }
            else
            {
                //
                // Display the new IP address information.
                //
                GrStringDraw(&g_sContext, "IP Address:", -1, 60, STATUS_Y,
                             false);
                GrStringDraw(&g_sContext, "Subnet Mask:", -1, 60, STATUS_Y + 20, false);
                GrStringDraw(&g_sContext, "Gateway:", -1, 60, STATUS_Y + 40, false);
                DisplayIPAddress(ui32NewIPAddress, ui32Width / 2, STATUS_Y);
                DisplayIPAddress(lwIPLocalNetMaskGet(), ui32Width / 2, STATUS_Y + 20);
                DisplayIPAddress(lwIPLocalGWAddrGet(), ui32Width / 2,
                                 STATUS_Y + 40);
            }
    
            //
            // Save the new IP address.
            //
            g_ui32IPAddress = ui32NewIPAddress;
        }
    
        //
        // If there is not an IP address, draw the animated circle.
        //
        if((ui32NewIPAddress == 0) || (ui32NewIPAddress == 0xffffffff))
        {
            //
            // Loop through the circles in the animation.
            //
            for(ui32Idx = 0; ui32Idx < 8; ui32Idx++)
            {
                //
                // Draw this circle.
                //
                GrContextForegroundSet(&g_sContext,
                                       g_pui32CircleColor[(g_ui32ColorIdx +
                                                           ui32Idx) & 7]);
                GrCircleFill(&g_sContext,
                             (ui32Width / 2) + g_ppi32CirclePos[ui32Idx][0],
                             STATUS_Y + g_ppi32CirclePos[ui32Idx][1] + 44,
                             2);
            }
    
            //
            // Increment the color index.
            //
            g_ui32ColorIdx++;
        }
    }
    
    //*****************************************************************************
    //
    // This example demonstrates the use of the Ethernet Controller and lwIP
    // TCP/IP stack to control various peripherals on the board via a web
    // browser.
    //
    //*****************************************************************************
    int
    main(void)
    {
        uint32_t ui32User0, ui32User1, ui32AnimPos, ui32Color;
        uint8_t pui8MACArray[8];
        tRectangle sRect;
        //
        // Run from the PLL at 120 MHz.
        //
        g_ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
                                             SYSCTL_OSC_MAIN |
                                             SYSCTL_USE_PLL |
                                             SYSCTL_CFG_VCO_480), 120000000);
    
        //
        // Configure the device pins.
        //
        PinoutSet();
    
        //
        // Initialize the display driver.
        //
        Kentec320x240x16_SSD2119Init(g_ui32SysClock);
    
        //
        // Initialize the graphics context.
        //
        GrContextInit(&g_sContext, &g_sKentec320x240x16_SSD2119);
    
        //
        // Draw the application frame.
        //
        FrameDraw(&g_sContext, "enet-io");
    
        //
        // Configure SysTick for a periodic interrupt.
        //
        ROM_SysTickPeriodSet(g_ui32SysClock / SYSTICKHZ);
        ROM_SysTickEnable();
        ROM_SysTickIntEnable();
    
        //
        // Configure the hardware MAC address for Ethernet Controller filtering of
        // incoming packets.  The MAC address will be stored in the non-volatile
        // USER0 and USER1 registers.
        //
        ROM_FlashUserGet(&ui32User0, &ui32User1);
        if((ui32User0 == 0xffffffff) || (ui32User1 == 0xffffffff))
        {
            //
            // We should never get here.  This is an error if the MAC address has
            // not been programmed into the device.  Exit the program.
            //
            GrContextForegroundSet(&g_sContext, ClrRed);
            GrStringDrawCentered(&g_sContext, "MAC Address", -1,
                                 GrContextDpyWidthGet(&g_sContext) / 2,
                                 (GrContextDpyHeightGet(&g_sContext) / 2) - 4,
                                 false);
            GrStringDrawCentered(&g_sContext, "Not Programmed!", -1,
                                 GrContextDpyWidthGet(&g_sContext) / 2,
                                 (GrContextDpyHeightGet(&g_sContext) / 2) + 16,
                                 false);
            while(1)
            {
            }
        }
    
        //
        // Tell the user what we are doing just now.
        //
        GrStringDrawCentered(&g_sContext, "Waiting for IP", -1,
                             GrContextDpyWidthGet(&g_sContext) / 2,
                             STATUS_Y, false);
    
        //
        // Draw the box inside which a text string sent from browser will be
        // displayed.
        //
        sRect.i16XMin = 10;
        sRect.i16XMax = GrContextDpyWidthGet(&g_sContext) - sRect.i16XMin - 1;
        sRect.i16YMin = TEXT_BOX_TOP;
        sRect.i16YMax = TEXT_BOX_BOTTOM - 1;
        GrContextForegroundSet(&g_sContext, ClrWhite);
        GrRectDraw(&g_sContext, &sRect);
        GrContextFontSet(&g_sContext, g_psFontCmss18);
        GrStringDraw(&g_sContext, " Browser Text: ", -1, sRect.i16XMin + 6,
                     TEXT_BOX_TOP - 10, true);
    
        //
        // Draw the box inside which we will draw the animation.
        //
        sRect.i16XMin = ANIM_LEFT;
        sRect.i16XMax = (ANIM_LEFT + ANIM_WIDTH) - 1;
        sRect.i16YMin = ANIM_TOP;
        sRect.i16YMax = (ANIM_TOP + ANIM_HEIGHT) - 1;
        GrContextForegroundSet(&g_sContext, ClrWhite);
        GrRectDraw(&g_sContext, &sRect);
    
        //
        // Initialize the animation variables.
        //
        ui32AnimPos = ANIM_LEFT + 1;
        ui32Color = ClrRed;
    
        //
        // Convert the 24/24 split MAC address from NV ram into a 32/16 split
        // MAC address needed to program the hardware registers, then program
        // the MAC address into the Ethernet Controller registers.
        //
        pui8MACArray[0] = ((ui32User0 >>  0) & 0xff);
        pui8MACArray[1] = ((ui32User0 >>  8) & 0xff);
        pui8MACArray[2] = ((ui32User0 >> 16) & 0xff);
        pui8MACArray[3] = ((ui32User1 >>  0) & 0xff);
        pui8MACArray[4] = ((ui32User1 >>  8) & 0xff);
        pui8MACArray[5] = ((ui32User1 >> 16) & 0xff);
    
        //
        // Initialze the lwIP library, using DHCP.
        //
        lwIPInit(g_ui32SysClock, pui8MACArray, 0, 0, 0, IPADDR_USE_DHCP);
    
        //
        // Setup the device locator service.
        //
        LocatorInit();
        LocatorMACAddrSet(pui8MACArray);
        LocatorAppTitleSet("DK-TM4C129X enet_io");
    
        //
        // Initialize a sample httpd server.
        //
        httpd_init();
    
        //
        // Set the interrupt priorities.  We set the SysTick interrupt to a higher
        // priority than the Ethernet interrupt to ensure that the file system
        // tick is processed if SysTick occurs while the Ethernet handler is being
        // processed.  This is very likely since all the TCP/IP and HTTP work is
        // done in the context of the Ethernet interrupt.
        //
        ROM_IntPrioritySet(INT_EMAC0, ETHERNET_INT_PRIORITY);
        ROM_IntPrioritySet(FAULT_SYSTICK, SYSTICK_INT_PRIORITY);
    
        //
        // Pass our tag information to the HTTP server.
        //
        http_set_ssi_handler((tSSIHandler)SSIHandler, g_pcConfigSSITags,
                             NUM_CONFIG_SSI_TAGS);
    
        //
        // Pass our CGI handlers to the HTTP server.
        //
        http_set_cgi_handlers(g_psConfigCGIURIs, NUM_CONFIG_CGI_URIS);
    
        //
        // Initialize IO controls
        //
        io_init();
    
        //
        // Loop forever, processing the on-screen animation.  All other work is
        // done in the interrupt handlers.
        //
        while(1)
        {
            //
            // Wait for a new tick to occur.
            //
            while(!g_ulFlags)
            {
                //
                // Do nothing.
                //
            }
    
            //
            // Clear the flag now that we have seen it.
            //
            HWREGBITW(&g_ulFlags, FLAG_TICK) = 0;
    
            //
            // Update the bar position and check for wrap.
            //
            ui32AnimPos ++;
            if(ui32AnimPos == ((ANIM_LEFT + ANIM_WIDTH) - 1))
            {
                //
                // We've reached the right edge so change color and move back
                // to the left.
                //
                ui32AnimPos = ANIM_LEFT + 1;
                ui32Color += COLOR_INCREMENT;
            }
    
            //
            // Now we draw the new bar.  Note that we need to temporarily
            // disable the ethernet interrupt while doing this since we have
            // been naughty and set this app up so that it accesses the graphics
            // library from two different contexts.
            //
            ROM_IntDisable(INT_EMAC0);
            GrContextForegroundSet(&g_sContext, ui32Color);
            GrLineDrawV(&g_sContext, ui32AnimPos, (ANIM_TOP + 1),
                        (ANIM_TOP + ANIM_HEIGHT) - 2);
            ROM_IntEnable(INT_EMAC0);
        }
    }
    
    //*****************************************************************************
    //
    // io.c - I/O routines for the enet_io example application.
    //
    // Copyright (c) 2007-2013 Texas Instruments Incorporated.  All rights reserved.
    // Software License Agreement
    // 
    // Texas Instruments (TI) is supplying this software for use solely and
    // exclusively on TI's microcontroller products. The software is owned by
    // TI and/or its suppliers, and is protected under applicable copyright
    // laws. You may not combine this software with "viral" open-source
    // software in order to form a larger program.
    // 
    // THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
    // NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
    // NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
    // CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
    // DAMAGES, FOR ANY REASON WHATSOEVER.
    // 
    // This is part of revision 2.0.1.11577 of the DK-TM4C129X Firmware Package.
    //
    //*****************************************************************************
    #include <stdbool.h>
    #include <stdint.h>
    #include "inc/hw_ints.h"
    #include "inc/hw_memmap.h"
    #include "inc/hw_pwm.h"
    #include "inc/hw_types.h"
    #include "driverlib/gpio.h"
    #include "driverlib/pwm.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/timer.h"
    #include "driverlib/interrupt.h"
    #include "driverlib/rom.h"
    #include "utils/ustdlib.h"
    #include "io.h"
    
    //*****************************************************************************
    //
    // Hardware connection for the user LED.
    //
    //*****************************************************************************
    #define LED_PORT_BASE GPIO_PORTQ_BASE
    #define LED_PIN GPIO_PIN_7
    
    #define IO_PORT_BASE_N GPIO_PORTN_BASE
    #define IO_PIN_0 GPIO_PIN_0
    #define IO_PORT_BASE_P GPIO_PORTP_BASE
    #define IO_PIN_1 GPIO_PIN_6
    #define IO_PORT_BASE_B GPIO_PORTB_BASE
    #define IO_PIN_2 GPIO_PIN_4
    #define IO_PIN_3 GPIO_PIN_2
    
    //*****************************************************************************
    //
    // The system clock speed.
    //
    //*****************************************************************************
    extern uint32_t g_ui32SysClock;
    
    //*****************************************************************************
    //
    // The current speed of the on-screen animation expressed as a percentage.
    //
    //*****************************************************************************
    volatile unsigned long g_ulAnimSpeed = 10;
    
    //*****************************************************************************
    //
    // Set the timer used to pace the animation.  We scale the timer timeout such
    // that a speed of 100% causes the timer to tick once every 4 mS (250Hz).
    //
    //*****************************************************************************
    static void
    io_set_timer(unsigned long ulSpeedPercent)
    {
        unsigned long ulTimeout;
    
        //
        // Turn the timer off while we are mucking with it.
        //
        ROM_TimerDisable(TIMER2_BASE, TIMER_A);
    
        //
        // If the speed is non-zero, we reset the timeout.  If it is zero, we
        // just leave the timer disabled.
        //
        if(ulSpeedPercent)
        {
            ulTimeout = g_ui32SysClock / 250;
            ulTimeout = (ulTimeout * 100 ) / ulSpeedPercent;
    
            ROM_TimerLoadSet(TIMER2_BASE, TIMER_A, ulTimeout);
            ROM_TimerEnable(TIMER2_BASE, TIMER_A);
        }
    }
    
    //*****************************************************************************
    //
    // Initialize the IO used in this demo
    //
    //*****************************************************************************
    void
    io_init(void)
    {
        //
        // Configure Port F0 for as an output for the status LED.
        //
        ROM_GPIOPinTypeGPIOOutput(LED_PORT_BASE, LED_PIN);
        ROM_GPIOPinTypeGPIOOutput(IO_PORT_BASE_N, IO_PIN_0);
        ROM_GPIOPinTypeGPIOOutput(IO_PORT_BASE_P, IO_PIN_1);
        ROM_GPIOPinTypeGPIOOutput(IO_PORT_BASE_B, IO_PIN_2);
        ROM_GPIOPinTypeGPIOOutput(LED_PORT_BASE, IO_PIN_3);
    
        //
       // GPIODireModeSet(IO_PORT_BASE_B,IO_PIN_2, GPIO_DIR_MODE_OUT);
        // Initialize LED to OFF (0)
        //
        ROM_GPIOPinWrite(LED_PORT_BASE, LED_PIN, 1);
        ROM_GPIOPinWrite(IO_PORT_BASE_N, IO_PIN_0, 1);
        ROM_GPIOPinWrite(IO_PORT_BASE_P, IO_PIN_1, 1);
        ROM_GPIOPinWrite(IO_PORT_BASE_B, IO_PIN_2, 1);
        ROM_GPIOPinWrite(LED_PORT_BASE, IO_PIN_3, 1);
    
        //
        // Enable the peripherals used by this example.
        //
        ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER2);
    
        //
        // Configure the timer used to pace the animation.
        //
        ROM_TimerConfigure(TIMER2_BASE, TIMER_CFG_PERIODIC);
    
        //
        // Setup the interrupts for the timer timeouts.
        //
        ROM_IntEnable(INT_TIMER2A);
        ROM_TimerIntEnable(TIMER2_BASE, TIMER_TIMA_TIMEOUT);
    
        //
        // Set the timer for the current animation speed.  This enables the
        // timer as a side effect.
        //
        io_set_timer(g_ulAnimSpeed);
    }
    
    //*****************************************************************************
    //
    // Set the status LED on or off.
    //
    //*****************************************************************************
    void
    io_set_led(bool bOn)
    {
        //
        // Turn the LED on or off as requested.
        //
        ROM_GPIOPinWrite(LED_PORT_BASE, LED_PIN, bOn ? LED_PIN : 0);
    }
    
    //*****************************************************************************
    //
    // Return LED state
    //
    //*****************************************************************************
    void
    io_get_ledstate(char * pcBuf, int iBufLen)
    {
        //
        // Get the state of the LED
        //
        if(ROM_GPIOPinRead(LED_PORT_BASE, LED_PIN))
        {
            usnprintf(pcBuf, iBufLen, "ON");
        }
        else
        {
            usnprintf(pcBuf, iBufLen, "OFF");
        }
    
    }
    
    //*****************************************************************************
    //
    // Return LED state as an integer, 1 on, 0 off.
    //
    //*****************************************************************************
    int
    io_is_led_on(void)
    {
        //
        // Get the state of the LED
        //
        if(ROM_GPIOPinRead(LED_PORT_BASE, LED_PIN))
        {
            return(true);
        }
        else
        {
            return(0);
        }
    }
    
    //*****************************************************************************
    //
    // Set the speed of the animation shown on the display.  In this version, the
    // speed is described as a decimal number encoded as an ASCII string.
    //
    //*****************************************************************************
    void
    io_set_animation_speed_string(char *pcBuf)
    {
        unsigned long ulSpeed;
    
        //
        // Parse the passed parameter as a decimal number.
        //
        ulSpeed = 0;
        while((*pcBuf >= '0') && (*pcBuf <= '9'))
        {
            ulSpeed *= 10;
            ulSpeed += (*pcBuf - '0');
            pcBuf++;
        }
    
        //
        // If the number is valid, set the new speed.
        //
        if(ulSpeed <= 100)
        {
            g_ulAnimSpeed = ulSpeed;
            io_set_timer(g_ulAnimSpeed);
        }
    }
    
    //*****************************************************************************
    //
    // Set the speed of the animation shown on the display.
    //
    //*****************************************************************************
    void
    io_set_animation_speed(unsigned long ulSpeed)
    {
        //
        // If the number is valid, set the new speed.
        //
        if(ulSpeed <= 100)
        {
            g_ulAnimSpeed = ulSpeed;
            io_set_timer(g_ulAnimSpeed);
        }
    }
    
    //*****************************************************************************
    //
    // Get the current animation speed as an ASCII string.
    //
    //*****************************************************************************
    void
    io_get_animation_speed_string(char *pcBuf, int iBufLen)
    {
        usnprintf(pcBuf, iBufLen, "%d%%", g_ulAnimSpeed);
    }
    
    //*****************************************************************************
    //
    // Get the current animation speed as a number.
    //
    //*****************************************************************************
    unsigned long
    io_get_animation_speed(void)
    {
        return(g_ulAnimSpeed);
    }
    
    Hi Chuck, sure Thanks for your reply.

  • As you succeeded w/PN_0 only - is it not (almost) clear that you employed "1" as the 3rd (final) argument - w/in "ROM_GPIOPinWrite()?"

    Your entire code is unnecessary - employ the "bit weighted" value as parameter 3! (i.e. PN_1=2, PN_2=4...PN_7=128). You may also repeat (echo) the 2nd argument into the 3rd argument. (i.e. IO_PORT_BASE_N, IO_PIN_5, IO_PIN_5)

    Note IO_PORT_BASE_N, IO_PIN_5, 32) works as well...

    Success w/ P(x)_0 (only) proves a "Dead giveaway!"