when I debug project my TM4C1294 Connected LaunchPad,the CCS6.0 shows "Error connecting to the target".when I connect it to PC,the LaunchPad can be identified by PC,and all drives is normal ,but when debug program it shows above massage.It happens as this,last time I wanted to download program with the launchpad,I connected it with annother board I forgot to disconnect the power supply of the board,then I connect the launchpad and the launchpad connected PC,and the JP3 connected ,then the CCS showed "Error connecting to the target".since then,everytime useit , it always show error.I tryed to unlock the chip, but it is useless.AND BY THE WAY,THETM4C123 become alittle hot.what should I do to solve it???