Using: RM48L952ZWT with HalCoGen and CCS
I have a custom board, not the Hercules HDK, which adds 128Mb (16MB) SDRAM, which the EE and I configured. We were able to get the SDRAM working. We tested the SDRAM by creating a function, doRamTest()
boolean doRamTest()
{
uint32 *lpuRam = (uint32 *)0x80000000;
uint32 uRamCount = 0x1000000 / 4;
// Write the pattern.
uint32 uIndex = 0;
uint32 uData = 0xFFFFFFFF;
uint32 *lpuIndex = lpuRam;
for (uIndex = 0; uIndex < uRamCount; uIndex++)
{
*lpuIndex = uData;
uData--;
lpuIndex++;
}
// Verify the pattern.
uData = 0xFFFFFFFF;
lpuIndex = lpuRam;
for (uIndex = 0; uIndex < uRamCount; uIndex++)
{
if (uData != *lpuIndex)
return FALSE;
uData--;
lpuIndex++;
}
return TRUE;
}
The function successfully returns.
The CCS map file generated for my RM48L952ZWT Hercules chip with HalCoGen only uses the internal memory on the Hercules chip.
******************************************************************************
TI ARM Linker PC v5.2.7
******************************************************************************
>> Linked Mon May 30 08:27:51 2016
OUTPUT FILE NAME: <CCMv3.out>
ENTRY POINT SYMBOL: "_c_int00" address: 0003caa4
MEMORY CONFIGURATION
name origin length used unused attr fill
---------------------- -------- --------- -------- -------- ---- --------
VECTORS 00000000 00000020 00000020 00000000 X
FLASH0 00000020 0017ffe0 0005047b 0012fb65 R X
FLASH1 00180000 00180000 00000000 00180000 R X
STACKS 08000000 00001500 00000000 00001500 RW
RAM 08001500 0003eb00 000050d8 00039a28 RW
I am half expecting to see 2 RAM regions along with bigger allocations for everything. Here are our HalCoGen settings:
How do I get my development environment to make use of the SDRAM?