Hi
We are programming the 6965 processor from your standard utility (Build 1613)provided and also downloadable from forum. We downloaded latest version
Here is screenshot for your reference.
When we connect 6965 board one to one with my PC, the board is getting programmed. But when we are connecting it to the local network, we are unable to program it.
The screenshot is as shown below
It shows attempting to connect.
We are getting ping from the unit i.e. it is perfectly connected to LAN and we have already checked that TFTP port is opened on network.
We verified it by installing TFTP server on one machine and we sent one dummy file from the TFTP client from other machine connected on other VLAN.
We have installed many number of units across India and we should be able to program them on our virtual LAN.
Please provide us with details on which network protocols like TCP/UDP,ftp,sftp,etc and ports like 63,65,etc. needs to be opened.
Also We are trying to connect on local LAN where there is no issue of proxy or security. However the connection gets failed if connected via switch on local LAN.
Thanks and regards
Pradhan