Other Parts Discussed in Thread: EK-TM4C1294XL
Hi,
I have been having issues using IAR version 7.40 with the TM4C1294XL Launchpad. I can successfully download a build to the launchpad, but every single time I try to exercise any features of the debugger (such as single-step, run, stop, etc.), IAR freezes/crashes. It is acting like it cannot communicate to the launchpad via the JTAG interface. As soon as I disconnect the debugger and reset the launchpad, the downloaded build runs fine.
So, it definitely seems like the debugger is having issues talking to this board. Do you have any thoughts on what I can try to fix this? Debugger settings? Ways to reset the launchpad to default settings? Driver input? I have tried various different ICDI drivers all with no differing effect.
Thanks