Other Parts Discussed in Thread: TM4C1290NCPDT
Dear Sir/ Madam
Please find attached Sch for TIVA series controller as per discussion.
We have use the TIVA based Controller : TM4C1290NCPDT for our Calibrators,
For communication and Bootloading we have use the In built USB controller of the same.
Below are the issue/s regarding the compatibility of the Drivers with Windows 10 / 8 / 8.1.
1) TIVA ware USB serial Port is not being assigned by the CPU with Win 8 or higher.
Our input for the above issues.
1) We used drivers as same as in Win 7 which is compatible with controller . and it is working OK with windows 7
.
Expectation from your side:
1) As per in your reference document named: DK-TM4C123G Firmware Development Package attached in mail, your USB Serial Drivers is compatible with Windows XP, Windows Vista and Windows 7. We want the end solution for the compatibility issues in Win. 8 and higher whether by any patches or full proven drivers.
Awaiting for your support.
thanks in advance.
Pradhan