Other Parts Discussed in Thread: LM2576
Hello,
The custom board is working fine till 1 hour but after that the MCU gets damaged.
I have power section using LM2576 which convert 12V to 5V which is input to AMS1117 which convert 5V to 3.3V which is 3.3V supply to the MCU but after 1 hr or so the MCU's VCC and Gnd is getting short.
Am I making any mistake???
Kindly Help!!!!!!!
Regards,
Shaheen.