Other Parts Discussed in Thread: EK-TM4C129EXL, EK-TM4C1294XL
I'm running the senshub_iot example from tivaware - fresh download
I created an exocit account and added my launchpad with MAC address.
My launchpad receives an IP address from my router.
When connecting to the exocite url to receive the CIK, I get an http 404
Current MAC: 08:00:28:5a:83:b9 Welcome to the EK-TM4C1294XL Exosite Senshub IoT Demo using FreeRTOS! IP: 192.168.1.6 CIK not found in EEPROM. Connecting to exosite to obtain a new CIK... Attempt 1 of 3 to acquire CIK failed! Attempt 2 of 3 to acquire CIK failed! Attempt 3 of 3 to acquire CIK failed! No CIK could be obtained.
The http 404 is happening in file
exocite.c
line 291
http_status = get_http_status(sock);
if (200 == http_status)
{
Unrelated, but relevant because it's step 1 in the instructions:
There's also a 404 on the exosite home page in the browser:
When you're logged in, and under step 1
you click on:
Configure your device:
) gives a 404 too.