This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

please tell me where the ram parity stored at?



Dear All

Please tell me where the ram parity stored at? I didnt find the address for them in memory table.

Leo

  • Which part and which RAM (main, MibADC, DCAN, Flexray, ..) are you asking about?
  • Dear Bob
    I am working on "6.3.2 Support for Cortex-R4F CPU's Address and Control Bus Parity Checking" and its selftest routine, so I was asking about the main ram, where is the parity bits stored, I'd like to view them via debugger memory viewer.
    Leo
  • Dear Bob
    I happen to be looking at dma parity check now.
    I understand that after entering test mode parity bits are mapped to the control packet RAM starting address A00h.
    So my question is before entering test mode, where are the parity bits? Can I view them through debugger?
    Leo
  • Dear Bob
    I find another strange thing, it says that "there is one parity bit for 16 bits of the ADC RAM." in SPNU515B page 948.
    Actually I find that, the bit15 is the parity bit for bit0-14,
    I enabled writing to adc ram
    then I do (*(volatile uint32 *)0xFF3E0000U) = 0U; then I saw 1000000000000000 (binary) at that 0xFF3E0000U
    if i do (*(volatile uint32 *)0xFF3E0000U) = 1U; then I saw 0000000000000001 (binary)
    so for each 16bits in adc ram, 15bits are for data, the last bit is the parity bit of the first fifteen bits.
    If I am correct about this speculation, the user guide will wrong. Am I right?
    Leo
  • Sorry, too much questions. But I cannot stop asking.
    "The ADC RAM address which generated the parity error is captured for host system debugging, " SPNU515B page 948.
    but I find that ADPARADDR Register keeps 0 in my parity selftest routine.
    then I saw "In emulation mode, this address is maintained frozen even when read"
    Is emulation mode as same as selftest mode?
    Leo
  • Leo, that section is talking about a parity bit on the BTCM bus, the address and control signals between the RAM and the CPU. It is an additional bus signal therefore it is not visible by the debugger. The BTCM RAM has ECC and the location of those bits is documented in the datasheet (0x08400000). You never did tell me which part to are looking at.
  • The DMA parity bits are only visible in the TEST mode.