Other Parts Discussed in Thread: HALCOGEN
Hello,
I have installed the N2HET IDE and have sent the form for the SynaptiCAD License a few days ago; I have no response from SynaptiCAD. Is this something that should happen automatically? Do I need to talk to someone at SynaptiCAD?
According to some documentation I found, there should be a tutorial directory in the IDE folder; but I can't find it. Where should I be able to locate that?
Since I am asking this, may as well ask this too. I have seen a few posts on this but nothing that was complete. I need to calculate RPM based on a capture input to the N2HET pin assigned to the sensor. Worst case I thought I could config as a GPIO and count edges. But if there is an example; I would appreciate seeing it.
Thanks,
John W.