Other Parts Discussed in Thread: TMS5700332
I'm using a Hercules TMS5700332 and the TPS65381 watchdog. Using the SafeTI Diag library V 2.2.0. I make the call to TPS_DriverInit and this code gets stuck in an infinite loop
while (TPS_DEVICE_DIAGNOSTIC != u8tps_device_state)
{
blRetVal = TPS_GetCurrentTPSDeviceState(&u8tps_device_state);
}
I'm testing this in debug mode in CCS and I understand that perhaps I'm taking longer than 600ms to get to the Active state. But I'm surprised I never get out of safe mode (TPS_DEVICE_SAFE). Looking at the TPS device State Diagram on page 72 of the spec sheet it looks like after entering safe state it should exit if DEV_ERR_CNT <> SAFE_LOCK_THR + 1, I verified this is true in my case. I also looked at the ABIST and LBIST results and they passed.
Is it right that I will not be able to transition out of safe mode if I miss that 600 ms timeout window? I'm currently not configuring the tps device in the bootloader so maybe I need to in order to ensure I get to the Active state in less than 600ms?