This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ETH#03 in TM4C129x Silicon Errata(SPMZ850F)



Hello,

For ETH#03 in TM4C129x Silicon Errata(SPMZ850F),
I have a some questions.

1. JTAG may not work
There is a following of a such a description.
Also if a 25MHz crystal is used without RBIAS resistor, then JTAG may not work.
But, there is a following of a such a description in datasheet P.1941.
The internal Ethernet PHY should not be enabled when RBIAS is not connected.
The ROM boot loader will enable the internal Ethernet Phy if no code is present
in the flash and a 24-25Mhz crystal is attached to the OSC0/1 pins.

Regardless of the frequency of the external crystal, if there is no RBIAS resistance,
we understand the JTAG does not work. Is it a Correct?
Selected Crystal values: 24.576MHz(unuse EtherPHY)

2.RBIAS resistor value
As described in the errata, we connected to the 4.7KΩ ± 10% of the resistance
to RBIAS pin.
However, JTAG does not work. why?
What are the safe resistor value?

Potential problems
・Point-to-point construction


Best Regards,
sopatopa