Other Parts Discussed in Thread: HALCOGEN
Project: I have to generate some digital signal (frequency from 1Khz to 10Mhz) and then need to develop both CAN & LIN protocol generation & analyzer circuits.
There is a c2000 microcontroller F28035, which supports both CAN and LIN , but its lunchpad is not available. I can use its Experimenter Kit, but the cost of buying it is much higher than that of Launchpad.
I also checked Herculus Launchpad, and it was looking good for my requirement. I am still confused to choose one between c2000 and Herculus.
I have to also build a GUI for both CAN and LIN . I have only used MSP432 launchpad so i am also not sure which will be easy to code either c2000 or Herculus.
Please guide me.
Thanks,
Neeraj