looking to use the Hercules in an automotive safety app.
Wanted the device to be able to read/write to a 1 wire eeprom..(per customer spec)...as a key
So..
One Hercules (on a remote system) would generate a random number when the 1-wire is connected...write the number to the device...store that number
the device would then be moved to another Hercules (on other remote control system). the Hercules would read the device then send that "key" ...the original Hercules then sees the key and knows they are legite and connected...
not sure if the device would have to be "bit banged", or maybe the spi module can handle it. (haven't gone to deep into datasheets for Hercules).
(have used the TIVA before for other things...but not the Hercules)
doable?
thanks