Hello all. By following the schematics and information found in the TI's EK-TM4C1294XL Connected Launchpad User's Guide, I'm trying to design/built a new breakout board for the TM4C1294NCPDT processor without the debug interface, user switches, LEDs and power options. I need to keep only the the IP and the magnetics on-board as is and also to use an external 5V 3A power feed for the board. Also I need to have many of the GPIOs streamed onto X-style BoosterPack or VALVANO's style pin-outs. Is there already any board of this or of similar type in the market? Are there already some schematics for such a board or the only available material is the pre-mentioned TI's user's guide? Would someone have to suggest a PCB/prototyping services company for that purpose? Thank you very much. John