This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Confusion with TivaWare 2.1.2.111 CAN Example

In TivaWare 2.1.2.111, the file example/peripherals/can/simple_tx.c has the following code

uint32_t ui32MsgData;
uint8_t *pui8MsgData;

pui8MsgData = (uint8_t *)&ui32MsgData;

. . . . 

//
// Initialize the message object that will be used for sending CAN
// messages. The message will be 4 bytes that will contain an incrementing
// value. Initially it will be set to 0.
//
ui32MsgData = 0;
sCANMessage.ui32MsgID = 1;
sCANMessage.ui32MsgIDMask = 0;
sCANMessage.ui32Flags = MSG_OBJ_TX_INT_ENABLE;
sCANMessage.ui32MsgLen = sizeof(pui8MsgData);
sCANMessage.pui8MsgData = pui8MsgData;



This line

sCANMessage.ui32MsgLen = sizeof(pui8MsgData);

 should read

sCANMessage.ui32MsgLen = sizeof(ui32MsgData);

One is not specifying the length of the pointer pui8MsgData, but the length of the buffer it points to.

It just happens that both are the same, so the code works. But that's not what the code says.