HI Bob, Anthony suggested that I post this question in the forum, as you are the expert in this area. Anthony phased the following question:
I would just tell him that you:
a) understand there is a PLL errata
b) don't need to use the PLL because you are directly running from the oscillator input at 20MHz.
c) would like to know what settings in HalCoGen can be used to completely skip the PLL initialization (so you avoid having any chance of waiting for it to lock when it may not...)