This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Real time Debugging TI Stellaris TM4C123 with IAR EW ARM

Hi All,

I want to monitor my application's global variable on run time using TI TM4C123G launchpad which comes with Stellaris ICDI debugger. But when I want to enbale live watch on IAR EW for ARM it is disabled. My question is does stellaris ICDI debugger support real time debugging, I mean live watch of global variables inside IAR EW. 

Is there any way to live watch wit Stellaris ICDI debugger, or I should move to other debugger like segger JLink.

Thanks

Sattar Malokani

  • Hello Sattar

    I don't think that it is a debugger issue, but more of an issue with the IDE

    Regards
    Amit
  • SATTAR MALOKANI said:
    want to monitor my application's global variable on run time using TI TM4C123G launchpad which comes with Stellaris ICDI debugger.

    You are correct in your observations - to enable IAR's "Live Watch" (which is extremely powerful) you DO require a proper JTAG/SWD probe/pod.   (such as J-Link or better)   Note that the J-Link is sold by Segger at great discount via their "educational program."   And - you do not have to, "Swear to student status" to obtain the substantial discount - simply comply w/Segger's fairly liberal usage requirements.

    We note that J-Link users are FAR less plagued w/Loss of Connection issues which appear to run rampant w/vendor's (lesser) implementation.

  • And Segger has additional live monitoring tools that do not require a running IDE.

    Robert