This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I have the trouble in running of bootloader with TFTP (bl_emac.c)



I've tried to build bootloader of EK_TM4C1294XL with enabling EMAC for using TFTP

Finally, I have managed to get TFTP data from TFTP server but the image is never fused to application of area of flash even though flash erase and program routine are called.

Are there someone who have succeed to fusing applcation program with bootloader enabled bl_emac.c (TFTP) ?

Please let me know success information 

- I'm using TivaWare_C_Series-2.1.2.111 & importing boot_serial project from example of EK_TM4C1294XL and changed some define value of bl_config.h as attached file.

Best Regards,

JY Koh4544.bl_config.h