This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kentec 3.5" display problem with TivaC T4M123

Other Parts Discussed in Thread: ENERGIA, CC3200

Hello,

I just got a Kentec 3.5" booster pack from TI (www.ti.com/.../BOOSTXL-K350QVG-S1) and I've been trying to interface it with a TivaC TM4C123 LaunchPad, I've tried it with multiple examples using TI Graphics library (GRLIB) and Energia (using EducationalBP_MKII examples) but no luck at all, nothing was displayed even the backlight wasn't working, like the backlight blinked once or twice when connecting the BoosterPack to the LP.

My question is: do I need to modify anything in the BP hardware prior to connecting it to the LP?, isn't incompatible with any LP except the SimpleLink CC3200 (I know it's not compatible with the CC3200, and I'm not using this LP for clarification).

Also, if you know a working example for this BP with any TI LaucnPad it will be highly appreciated if you can direct me to it.

Thanks,

Karim