This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PBIST memory test for TMS5703137DZWTQQ1

In order to perform memory test of PBIST, could you please provide the processing time when selecting following memory area?

If the processing time is represented by the number of cycles, please also let us know the type of standard clock.

 

                           MIBSPI1/ MIBSPI2/ MIBSPI3

CAN1/CAN2/CAN3

ADC1/ADC2

DMA/VIM

HET1/HTU1/HET2/HTU2

FLEXRAY SP RAM/FLEXRAY DP RAM

ESRAM

RTP

STC ROM

PBIST ROM

 

Thanks and Regards,

Taka