Other Parts Discussed in Thread: TMDSRM48HDK, UNIFLASH
Hello,
Connecting to TMDSRM48HDK works just great through built in XDS100v2 emulator, whether using CCS 6.1.2.00015 or UniFlash 3.4.1.00012. However, using an external XDS100v2 (TMDSEMU100V2U-14T) provides me the following error:
Same problem with CCS, except the emulation package is 6.0.83.1.
I have used the following pinout:
HDK-J4 ----- XDS100v2
1 ----- 5
2 ----- NC
3 ----- 2
4 ----- 8, 10, 12
5 ----- 3
6 ----- NC
7 ----- 1
8 ----- 8, 10, 12
9 ----- 11
10 ----- 8, 10, 12
11 ----- 9
12 ----- 8, 10, 12
13 ----- 7
14 ----- 8, 10, 12
15 ----- NC
16 ----- 8, 10, 12
17 ----- NC
18 ----- 8, 10, 12
19 ----- NC
20 ----- 8, 10, 12
Because the signal nSRST is not present on the 14 pin, I have added a wire from the test pad T_SRST_N to J14-15. Still doesn't work.
With the utility xds100serial, every parameters are the same between the built-in or external XDS100v2, except the serial numbers: built-in: TIMCUHDK, external:SD05YVRO.
I really need help to resolve this issue, since in production, there will be obviously no built-in XDS100v2 on our boards, and the processors must be programmed with an external emulator.
Thanks,
Hugues