Other Parts Discussed in Thread: HALCOGEN, RM48L952
The datasheet for the RM48L952ZWT states:
Internal Memory:
- 3MB of Program Flash With ECC
- 256KB of RAM With ECC
- 64KB of Flash with ECC for Emulated EEPROM"
I will take this block to mean that I have 64KB of dedicated emulated EEPROM specifically for use as EEPROM.
Halcogen in the FEE tab allows me up to 16 (one based) blocks. (I am using 10).
What is the maximum size in bytes that any one block can have?
Are there any restrictions on specifying block size (must be even, or in multiples of 32, or whatever)?