Other Parts Discussed in Thread: HALCOGEN
Hello,
I am using a Launchpad XL2 and I am trying to configure CAN. As clock configuration I am using the default values from Halcogen for my processor (RM46L852PGE).I did configure a bitrate of 50 kBit with Halcogen. I am sending CAN Tx frames and I am measuring these frames on a scope. I see the bitclock is not as expected 50kBit but around 36kBit. It seems as if the clock input for the CAN modules is somehow slower than expected from the processor. The clock input for CAN is VCLKA1 and the input for VCLKA1 is VCLK. (Everything as generated by HalcoGen).
Any ideas?
best regards
Matthias