Other Parts Discussed in Thread: BOOST-CCEMADAPTER
-
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Patrick,
Sorry for the delay in response. Some how this post got missed.
Is this the adapter board you are using: 
If yes, then did you make sure that the GPIOs from the LaunchPad are being connected to the CC1200EMK.
Although the BOOST-CCEMADAPTER is supposed to make the right connections, one of colleagues, who used the BOOST-CCEMADAPTER board, had to make some hardware adjustments. Although, I am not sure if the SPI pins were the issue.
Also while pasting code, can you use the syntax highlighter (it can be accessed by clicking on "Use rich formatting" and then the icon
).
Thanks,
Sai