Other Parts Discussed in Thread: TM4C123GH6PZ
Hello,
I am curious what functions the brown-out reset (BOR) is protecting against on the TM4C123GH6PZ. We have 32 complete systems (which use the TM4C123GH6PZ on one PCBA) running 24/7 reliability cycling, and just recently 2 of them started having BOR events about twice a day.
In reading the datasheet, I saw the BOR0 threshold is pretty tight (max 3.11V). In addition, there is a note beneath Table 24-10 stating:
"Digital logic, Flash memory, and SRAM are all designed to operate at VDD voltages below 2.70 V. The internal POK reset protects the device from unpredictable operation on power down."
After reading that, I am wondering what the purpose of the BOR reset is? The only thing I can think of is if the micro were communicating with a part in a different power system, and hence a brown-out could momentarily cause misinterpreted logic levels.
Thoughts? Am I risking damage to the TM4C123 by disabling either or both of the BORs?
Thank you in advance.