Other Parts Discussed in Thread: TMS570LS3137, HALCOGEN
Hello Team,
Can you please advise on possible causes or debug steps for the TMS570LS3137 for the following error (code gets stuck here at the beginning of a debug session):
/* Check if there were ESM group3 errors during power-up.
* These could occur during eFuse auto-load or during reads from flash OTP
* during power-up. Device operation is not reliable and not recommended
* in this case.
* An ESM group3 error only drives the nERROR pin low. An external circuit
* that monitors the nERROR pin must take the appropriate action to ensure that
* the system is placed in a safe state, as determined by the application.
*/
if ((esmREG->SR1[2]) != 0U)
{
/* USER CODE BEGIN (24) */
/* USER CODE END */
/*SAFETYMCUSW 5 C MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
/*SAFETYMCUSW 26 S MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
/*SAFETYMCUSW 28 D MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
for(;;)
{
}/* Wait */
/* USER CODE BEGIN (25) */
/* USER CODE END */
}
Thanks,
Casey McCrea