I keep trying to record data from the Sensor Hub Booster Pack into an SD card, for this reason i would really like to combine those examples.
What i tried is to put the code from the pressure_bmp180.c into de fatSD example from RTOS.
So the thing is that I could call the funcions to use the BPM180 APIs into the fatSD example, i just had to erase the ROM berore every function and it buids and shows no errors, ¡BUT IT DOSENT WORK!.
Then I runed it step by step in the disassembly window and found the line when it brokes. That line is in the initBMP180 API when the code gets there it just show no more lines in the disassembly window.
Any advice is helpful.
My host is windows 7
Using the EK-TM4C123GXL and CCS_6.1.2.00015.
. It's very hard to read code when it is in plain text.