Hi,
I need to know when the Cortex resets because the watchdog was not serviced on time so I can reset the board.
Is there a way to configure a pin to toggle when the watchdog trigger?
Khaled
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I need to know when the Cortex resets because the watchdog was not serviced on time so I can reset the board.
Is there a way to configure a pin to toggle when the watchdog trigger?
Khaled
I can't see a direct way make the watchdog toggle a pin when the watchdog triggers a reset.khaled saab said:I want to toggle the pin when the watchdog triggers a Cortex reset i.e. when the watchdog is not serviced on time.
Maybe an indirect method will work. E.g.:
a) Attach an external pull-up resistor on a spare GPIO.
b) When the software starts running it outputs a low on the GPIO.
c) When the watchdog triggers a Cortex reset, the GPIO will be tri-stated and will be pulled up externally, thus giving an external indication that a reset has occurred.
Not sure how quickly the GPIOs are tri-stated when the watchdog triggers a Corex reset.
One limitation with this indirect method is that can't tell the difference between the watchdog triggering a Cortex reset, or any other reset reason.
I'm not sure that it will work if we do it every time.
The point is that I want a WDG output pin that asserts when ever the Cortex resets and attach that WDG pin to the board reset circuitry.
I would like to avoid a closed loop reset i.e. the Cortex WDG triggers that triggers a board reset that triggers a Cortex reset that triggers a second "WDG pin" reset....
But from all of your inputs and looking more at the Cortex pins, it seems that there is no true WDG pin.
thanks for all of your inputs.
Khaled.
Khaled,
If I recall correctly, the watchdog interrupt on a typical configuration will be called once to"give you a chance of knowing something went wrong".
Then, if the timer rolls again, it will reset the MCU.
Assuming that the first watchdog timeout should actually never happen, and your application should have been designed in a way as to not let the dog starve, I'd suggest that you simply suicide the board inside the interrupt handler:
dogIntHandler(void)
{
GPIOPinWrite(boardResetLineBase, boardResetLinePin, boardResetLinePin);
SysCtlDelay(someTimeToResetYourBoard);
SysCtlReset();// Suicide
while(1);// Just in case
}
Regards,
Bruno
khaled saab said:I'm not sure that it will work if we do it every time.
If your board reset does not work every time, that's a big problem. I would address that as a high priority item.
khaled saab said:I would like to avoid a closed loop reset i.e. the Cortex WDG triggers that triggers a board reset that triggers a Cortex reset that triggers a second "WDG pin" reset....
That's primarily a h/w issue on your reset circuitry. Your micro's reset out should not reset the micro. ever.
And a primary reset will clear the watchdog, pretty much by definition.
khaled saab said:But from all of your inputs and looking more at the Cortex pins, it seems that there is no true WDG pin.
I've never seen a micro with one. I have seen them with reset out but the reset out is asserted regardless of the reset source.
I think you've confused your self about the way a board reset works. If you have a board reset to set the external devices to a known state you can drive it from the external reset (I.E. from your external supervisory IC) but the board reset should not feed back to the micro reset input.
Reset sources are diode ored so that the reset sources do not interfere. The board reset signal could be a diode or of the reset out from the micro and the supervisory IC, while the micro would come only from the supervisory IC.
Alternately the board reset only comes from the micro, not any external reset. Since you always reset the board on the micro reset you put the H/W in a known state before using. In this arrangement you lose the power-on reset and have a short period on startup before the board peripherals are reset. Only you know if this is significant enough to push you to a diode ored solution.
In either case it is quite possible with no worries about circular reset chains.
Robert
khaled saab said:You are correct. I could add a supervisory IC
I wasn't suggesting that. It's just that the only way you run into a circular reset problem is if you deliberately connect a reset out to the reset in.
khaled saab said:But I wanted the watchdog timeout to assert of the WDGOUT pin that will be OR'ed with the remaining reset inputs but not going to back to the micro it self.
That is very doable as I explained.
What you haven't explained is why it is worth restricting it to a watchdog only. I don't understand why you don't want the board to be consistent regardless of the reset source.
Robert
khaled saab said:all other resets are routed/hardwired to our system reset and I did not want to create a conditions for possible "loop" reset.
I think you are over-thinking this.
If a loop is possible in the case of other resets it is surely possible in the case of a watchdog. The electrical connections have not changed.
It neither case should a reset out from the processor drive a reset in. In neither case should the watchdog be active immediately after reset from any source.
Far more robust not to have your reset process be conditional on how you get to it.
Robert