This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123gh6pm UARTFR :what is the need of having TXFE ,TXFF also RXFE,RXFF ?



Please correct if I am wrong.

If TXFE=0---FIFO is not empty(full)

and TXFF=1--FIFO is full (not empty)

then what is the need of two separate bits(TXFF,TXFE) ?

Same for RX also .

Please explain!

  • From the User Manual

    TxFE

    UART Transmit FIFO Empty

    The meaning of this bit depends on the state of the FEN bit in the

    UARTLCRH register.

    Value Description

    0 The transmitter has data to transmit.

    1 If the FIFO is disabled (FEN is 0), the transmit holding register

    is empty.

    If the FIFO is enabled (FEN is 1), the transmit FIFO is empty

     

    TxFF

    UART Transmit FIFO Full

    The meaning of this bit depends on the state of the FEN bit in the

    UARTLCRH register.

    Value Description

    0 The transmitter is not full.

    1 If the FIFO is disabled (FEN is 0), the transmit holding register

    is full.

    If the FIFO is enabled (FEN is 1), the transmit FIFO is full.

    Obviously quite different meanings

    Four distinct possibilities

    TxFE, TxFF both 0 Not empty, not full

    TxFE 1, TxFF 0 Empty, not full

    TxFE 0, TxFF 1 not Empty, Full

    TxFE, TxFF both 1. This would indicate both full and empty and thus is not a legal state. The others all have obvious distinct meanings though

    Robert

  • Thanks Robert !

    Yeah I got now.TXFE=1 mean no data in fifo but it does not mean whenever TXFF=0 ,the fifo is completely Empty.

    thanks