Other Parts Discussed in Thread: DRV8301
Hi,
I have a problem with the GUI of DRV8301-LS31-KIT. I copied the folder DRV8301_TMS570LS31_BLDC in "C:\ti\guicomposer\webapps", connected the control card, then I launched "launcher.exe" but the GUI is stuck on program loading:
Restarting Program Model...
Initializing target : C:\ti\guicomposer\webapps\DRV8301_TMS570LS31_FOC_SMO_wEncoder\appConfig.ccxml
Connecting target: Texas Instruments XDS100v2 USB Emulator_0/CortexR4
Loading program: C:\ti\guicomposer\webapps\DRV8301_TMS570LS31_FOC_SMO_wEncoder\appProgram.out
No change after 15 minutes, I cannot change any setting in the Application part ("The target has not been initialized"). However, I can import the CCS project and run it on the board without problem. I would like to display the GUI though.
I use the GUIComposer-1.6.0.0 from the installation disk, on Windows 7 x64. I tried several other versions but they only made things worst (awful display).
Does someone have an idea of what might be wrong here?
Thanks,
Nam