I refer to page 1556 in SPNU515B, which is the TRM for a TMS570. I am unsure about "Input data is latched ..." in Table 28-2. Does it refer to the data from the master or from the slave? If it refers to the data from the master, I would expect a different wording, something like "The slave shall latch the data ...", and I would also not expect two traces with data in the four figures below. If it refers, however, to data from the slave, I wonder how the slave can drive D7 just before the first edge of the clock (Figures 28-9 and 28-11).