This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDS100V2 error in CCS V5.4.x



Hi,

I have developed a daughter card for RM48HDK. It uses the data and address lines and some IOs available on the expansion connectors of RM48HDK. 

When I plug the daughter card and then porgram the HDK, I get this error,

Error -241@0x0

A router subpath could not be accessed

A security error has probably occurred

(Emulation package 0.0.0.0)


Then it prompts to try again and following error occurs:

Error -1265@0x0

--------------------

The target connection works fine without the daughter card, what might be the problem and how to fix it.

I am using CCS Ver 5.4.x, Windows 7 or XP 

Any help would be highly appreciated.

Thanks

Anila