Hi,
Short version
Can I get an RM44L520 to read data bursts from an ADC at 40 MHz? If so, what kind of clock speeds does the MCU have to run at to manage this?
The data comes out of the ADC as parallell data, the bursts are 2.5 uS (100 samples) long, but there are multiple bursts (32 bursts) in sequence.
Longer version
The system we are designing generates an 250 nanosecond long RF pulse, switches the system from transmission to listen, and after approx 1 microsecond, starts reading from the ADC. The ADC outputs the baseband of the RF signal in two channels at 9 bit each.
The data bursts coming out of the ADC are 2.5 microseconds long.
The plan is to use the HET to generate the control signals for the RF pulse and then store the data from the two channels in two FIFOs, external to the MCU.
Write enable signals to the FIFOs will also be controlled from the HET.
However, I am thinking that maybe I can skip the FIFOs and write data straight into the MCU.
There are some more details than this involved, but is this even possible?
And what clock speed does the MCU need? Can it do this at less than 80 MHz, or does it have to run far faster than the ADC to manage this?
Best Regards
Audun Lonmo Knudsrod
R&D Engineer, Kongsberg Maritime