We've recently designed a new board using the TM4C129 processor and are having a hard time getting the micro to stay in hibernation. We have a lithium coin cell connected to VBAT and a 3.3V switched supply connected to VDD. We have a 1Meg pullup resistor connected to the lithium voltage on the WAKE pin. When we issue the hibernation command, the HIB~ signal activates for a little over 3 milliseconds then goes high. Startup code tells us that hibernation mode is no longer active and that a POR reset has occurred. Any thoughts as to why this is happening? One interesting note is that if I leave the VDD power on, the unit will go into hibernation and stay there.