Hi,
I have custom software running with TiRTOS on a TM4C1264NCPDT and I want to run the ROM_updateUSB(0) from my code in order to get into DFU mode and do a firmware update.
There are several posts about this and this is the code I am using derived from these posts...
//----------------------------------------------------------------------------------- void enterBootloader(void) { int ui32Addr; ROM_IntMasterDisable(); ROM_SysTickIntDisable(); ROM_SysTickDisable(); ROM_SysCtlPeripheralDisable(SYSCTL_PERIPH_USB0); HWREG(NVIC_DIS0) = 0xffffffff; HWREG(NVIC_DIS1) = 0xffffffff; HWREG(NVIC_DIS2) = 0xffffffff; HWREG(NVIC_DIS3) = 0xffffffff; HWREG(NVIC_DIS4) = 0xffffffff; for(ui32Addr = NVIC_PRI0; ui32Addr <= NVIC_PRI34; ui32Addr+=4) { HWREG(ui32Addr) = 0; } HWREG(NVIC_SYS_PRI1) = 0; HWREG(NVIC_SYS_PRI2) = 0; HWREG(NVIC_SYS_PRI3) = 0; ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOL); // while(!ROM_SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOL)) { } ROM_GPIOPinTypeUSBAnalog(GPIO_PORTL_BASE, GPIO_PIN_6 | GPIO_PIN_7); ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_USB0); while(!ROM_SysCtlPeripheralReady(SYSCTL_PERIPH_USB0)) { } ROM_SysCtlPeripheralReset(SYSCTL_PERIPH_USB0); SysCtlUSBPLLEnable(); ROM_SysCtlDelay(40000000); ROM_IntMasterEnable(); ROM_UpdateUSB(0); while(1) { } }
I am calling this from the USBCDCD thread (the command to go into bootloader is a serial port message from the host).
My problem is that this does not appear to run the bootloader in DFU mode until I power-cycle it.
Can anybody tell me what I am doing wrong please.
Thanks
Richard