Other Parts Discussed in Thread: EK-TM4C1294XL
Hello,
I’m trying to connect two TM4C1294 MCUs through SSI in the legacy SPI mode.
However, when the master send two commands without a long delay between them, the slave doesn't receive the second one.
The attached archive contains the sample codes having this issue.
In ssi_master/main.c, the data sent by the master at lines 114-115 are observed by a logic analyzer, but the slave doesn’t receive them.
The problem disappears when line 153 is uncommented or a long delay is added (using ROM_SysCtlDelay).
The master is run on a custom board while the slave is on a TM4C1924 launchpad (EK-TM4C1294XL).
ssi.zip