Other Parts Discussed in Thread: TM4C1230H6PM
I have made a custom board using TM4C1230H6PM. I am using JTAG to load & debug the program into the board. The connections are made as shown in the picture below.
I am using the ICDI on TM4C123GXL launchpad load program into the board.
I tried using CCS v6, and it gives me error which says "Error connecting to target"
I tried using LMFlash programmer, and it gives me error "Error connecting to target - 0"
I have tried literally everything that this forum posts suggests, referred all documents relating to JTAG, but still no luck.
I have checked the pin to pin connections for all 4 JTAG signals - TCK, TMS, TDI and TDO. They are correct.
Somewhere in this forum, it was mentioned that the voltage on RESET pin after connection is made should be 3.3V, but here I am getting 2.7V. I tried using a different launchpad, and a different custom board, but still voltage is 2.7V.
How to diagnose this problem? What could have possibly gone wrong in this schematic?