Other Parts Discussed in Thread: ENERGIA
I recently bought the Educational Booster pack MkII and I can get all the example sketches in Energia working apart from the LCD.
I have tried all the Energia EduBPMKII_Screen examples and even tried writing my own drivers from the datasheet. I am using the booster pack with a Tiva C TM4C123GXL MCU and all I ever see with any sketch including the LCD sketches is the backlight on the LCD.
I am beginning to doubt whether the LCD controller is working correctly. The hardware SPI on the TM4C is definitely OK as I have previously used SSI0 to interface with my Nokia 5510 LCD.
I am using Energia Windows: Binary release version 1.6.10E18 (8/11/2016)
Is there anything else I can try before getting a replacement board?
Thanks,
Chris