Other Parts Discussed in Thread: BOOSTXL-K350QVG-S1, SW-TM4C
Hello, I am using the TM4C123gh6pm evaluation board along with CCS 6.1.2 and Tivaware 2.1.2.111.
I was hoping you could give me some pointers to what is causing a mismatch in the values of my outputs.
I use the following interruptions:
PINB0 Set to be triggered by both edges, connected to a zero crossing detection circuit. Triggers an interruption of Timer2A or Timer3A.
Timer2A Writes to PC4 or PC5 and triggers Timer4A
Timer3A Writes to PC6 or PC7 and triggers Timer4A
Timer4A Clears PC4 PC5 PC6 PC7
Hibernation Set to generate an interrupt at RTC match, writes to PB1, PB2, PB3, PD2, PD3, PD6, PE3, PE4, PF3, These are the outputs that do not match the value that is written to them.
The main cycle checks the ADC and compares the output to a variable called temp_obj, if its over that value it writes 1 to flag_tobj otherwise it writes 0.
So far I tried disabling the interrupts when the RTC interrupt is triggered, and my outputs have keep their values more consistely but ocassionaly other values show up.
Im using the LCD BOOSTXL-K350QVG-S1, could it be causing an interference?
This is the code that I use in the hibernate interrupt handler:
void Hibernate_Handler(void)
{
uint32_t ui32Status;
ui32Status = HibernateIntStatus(1);
HibernateIntClear(ui32Status);
IntPendClear(INT_GPIOB);IntPendClear(INT_TIMER2A);IntPendClear(INT_TIMER3A);IntPendClear(INT_TIMER4A);
IntDisable(INT_TIMER2A);IntDisable(INT_TIMER3A); GPIOIntDisable(GPIO_PORTB_BASE,GPIO_INT_PIN_0);
if(flag_tobj==1)
{
switch(Sig_Proceso) {
case 0x00 ://PF3 PA7
//3
Sig_Proceso=0x01;
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_6|GPIO_PIN_7, 0x7F);
GPIOPinWrite(GPIO_PORTB_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0xFF);
GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_6, 0xFF);
GPIOPinWrite(GPIO_PORTE_BASE, GPIO_PIN_3|GPIO_PIN_4, 0xFF);
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3, 0xF7);
Tiempo_Proceso=5;
HibernateRTCSet(0);
HibernateRTCMatchSet(0,HibernateRTCGet()+Tiempo_Proceso);
break;
case 0x01 : PB1 PB3 PA7
Sig_Proceso=0x02;
GPIOPinWrite(GPIO_PORTA_BASE, (GPIO_PIN_6|GPIO_PIN_7), 0x7F);
GPIOPinWrite(GPIO_PORTB_BASE, (GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3), 0xF5);
GPIOPinWrite(GPIO_PORTD_BASE, (GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_6), 0xFF);
GPIOPinWrite(GPIO_PORTE_BASE, (GPIO_PIN_3|GPIO_PIN_4),0xFF);
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3, 0xFF);
Tiempo_Proceso=5;
HibernateRTCSet(0);
HibernateRTCMatchSet(0,HibernateRTCGet()+Tiempo_Proceso);
break;
}
}else
{
Tiempo_Proceso=05;
HibernateRTCSet(0);
HibernateRTCMatchSet(0,HibernateRTCGet()+Tiempo_Proceso);
}
IntPendClear(INT_GPIOB);IntPendClear(INT_TIMER2A);IntPendClear(INT_TIMER3A);IntPendClear(INT_TIMER4A);
IntEnable(INT_TIMER2A);IntEnable(INT_TIMER3A); GPIOIntEnable(GPIO_PORTB_BASE,GPIO_INT_PIN_0);
}