Other Parts Discussed in Thread: RM57L843, UNIFLASH
My chip is RM57L843.
My MPU configuration is as below:
{
region 1:
0x00000000
0xFFFFFFFF
NORMAL_OINC_NONSHARED
PRIV_NA_USER_NA_NOEXEC
region 2:
0x00000000
0x003FFFFF
NORMAL_OINC_NONSHARED
PRIV_RO_USER_RO_EXEC
region 3:
0x08000000
0x0807FFFF
NORMAL_OINC_NONSHARED
PRIV_RW_USER_RW_EXEC
region 4:
0x08400000
0x0847FFFF
NORMAL_OINC_NONSHARED
PRIV_RW_USER_RW_NOEXEC
region 5:
0x30000000
0x30FFFFFF
STRONGLYORDERED_SHAREABLE
PRIV-RW_USER_RW_NOEXEC
region 6:
0x34000000
0x37FFFFFF
NORMAL_OINC_NONSHARED
PRIV_NA_USER_NA_NOEXEC
region 7:
0x60000000
0x63FFFFFF
STRONGLYORDERED_SHAREABLE
PRIV_RW_USER_RW_EXEC
region 8:
0x64000000
0x67FFFFFF
STRONGLYORDERED_SHAREABLE
PRIV_RW_USER_RW_EXEC
region 9:
0x68000000
0x6BFFFFFF
STRONGLYORDERED_SHAREABLE
PRIV_RW_USER_RW_EXEC
region 10:
0x80000000
0x87FFFFFF
NORMAL_OINC_NONSHARED
PRIVE_RW_USER_RW_EXEC
region 11:
0xF0000000
0xF07FFFFF
NORMAL_OINC_NONSHARED
PRIV_RW_USER_RW_NOEXEC
region 12:
0xFB000000
0xFBFFFFFF
DEVICE_NONSHAEABLE
PRIV_RW_USER_RW_NOEXEC
region 13:
0xFC000000
0xFCFFFFFF
DEVICE_NONSHAREABLE
PRIV_RW_USER_RW_NOEXEC
region 14:
0xFE000000
0xFEFFFFFF
DEVICE_NONSHAREABLE
PRIV_RW_USER_RW_NOEXEC
region 15:
0xFF000000
0xFFFFFFFF
DEVICE_NONSHAREABLE
PRIV_RW_USER_RW_NOEXEC
region 16:
0xFFF80000
0xFFFFFFFF
DEVICE_NONSHAREABLE
PRIV_RW_USER_RW_NOEXEC
}
Now, I transplant SafeRTOS to RM57L843.
My RM57_flash.icf is as below.
{
define symbol __ICFEDIT_intvec_start__ = 0x00000000;
define symbol __ICFEDIT_region_ROM_start__ = 0x00000020;
define symbol __ICFEDIT_region_ROM_end__ = 0x003FFFFF;
define symbol __ICFEDIT_region_RAM_start__ = 0x08001500;
define symbol __ICFEDIT_region_RAM_end__ = 0x0807FFFF;
define symbol __ICFEDIT_size_cstack__ = 0x1000;
define symbol __ICFEDIT_size_svcstack__ = 0x100;
define symbol __ICFEDIT_size_irqstack__ = 0x100;
define symbol __ICFEDIT_size_fiqstack__ = 0x100;
define symbol __ICFEDIT_size_undstack__ = 0x100;
define symbol __ICFEDIT_size_abtstack__ = 0x100;
define symbol __ICFEDIT_size_heap__ = 0;
define memory mem with size = 4G;
define region ROM_region = mem:[from __ICFEDIT_region_ROM_start__ to __ICFEDIT_region_ROM_end__];
define symbol __total_stack_size__ =
__ICFEDIT_size_cstack__ +
__ICFEDIT_size_svcstack__ +
__ICFEDIT_size_fiqstack__ +
__ICFEDIT_size_irqstack__ +
__ICFEDIT_size_abtstack__ +
__ICFEDIT_size_undstack__;
define region STACK = mem:[from 0x08000000 size __total_stack_size__];
define region RAM_region = mem:[from __ICFEDIT_region_RAM_start__ to __ICFEDIT_region_RAM_end__];
define symbol __region_DRAM_start__ = 0x80000000;
define symbol __region_DRAM_end__ = 0x807FFFFF;
define region DRAM_region = mem:[from __region_DRAM_start__ to __region_DRAM_end__];
define block HEAP with alignment = 8, size = __ICFEDIT_size_heap__ { };
initialize by copy { readwrite };
do not initialize { section .noinit };
define block __kernel_functions_block__ with alignment = 8, size = 0x8000 - 0x60
{ section __kernel_functions__ };
place at address mem:__ICFEDIT_intvec_start__ { readonly section .intvecs, block __kernel_functions_block__ };
place in ROM_region { readonly };
define block __kernel_data_block__ with alignment = 0x800, size = 0x800
{
section __kernel_data__,
section __kernel_nz_data__,
};
define block __safety_diagnosis_data_block__ with alignment = 0x400, size = 0x400
{ section __safety_diagnosis_data__ };
define block __safety_iec_data_block__ with alignment = 0x1000, size = 0x1000
{ section __safety_iec_data__ };
define block __specified_data_block__ with alignment = 0x20000, size = 0x20000
{ section __specified_data__ };
define block __idle_task_data_block__ with alignment = 0x20, size = 0x20
{
section __idle_task_data__,
section __idle_task_zero_data__
};
place in RAM_region
{
readwrite,
block __kernel_data_block__,
block __safety_diagnosis_data_block__,
block __safety_iec_data_block__,
block __specified_data_block__,
block __idle_task_data_block__,
block HEAP
};
place in DRAM_region { section DRAM };
export symbol __ICFEDIT_intvec_start__;
export symbol __ICFEDIT_region_ROM_start__;
export symbol __ICFEDIT_region_ROM_end__;
}
My task is set PRIVILEGED.
After I tried to burn the program into RM57L843, CPU seems to be locked. Because I can't burn any program into RM57L843 any more afterwards.
When I burned the program, the error message box will be popped up. refer to below.
"Error connecting to the target:
(Error -2062 @ 0x0)
Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 6.0.14.5)"
I tried to erase flash using UniFlash. When I clicked erase before releasing RST button in a little time on evaluation board, the flash seems to be connected, but failed in access RAM address. Error message is as below.
[11:34:54] Erasing flash sectors on Core 0 < Texas Instruments XDS100v2 USB Debug Probe/CortexR5 > ...
[11:34:54] Begin Erase Flash operation.
[11:34:54] CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0
[11:34:55] CortexR5: Erasing Flash memory...
[11:34:57] Target failed to read 0x08000000
[11:34:58] Operation Erase Flash returned.
How can I do something to solve this issue? How can I unlock the RAM access?
Is there something error for my MPU configuration?